Sager Electronics Announces Immediate Availability of 15, 20 and 30 Watt Medical DC/DC Converters from TRACO Power

NEW PRODUCT ANNOUNCEMENT

MIDDLEBOROUGH, Mass. – January 29, 2018 – Sager Electronics, a leading North American distributor of Interconnect, Electromechanical and Power components and provider of value-add solutions, is now stocking TRACO Power’s THM 15WI, THM 20WI and THM 30WI medical DC/DC converters. 

These 15, 20 and 30 Watt DC/DC converters provide a reinforced insulation system for 5000 VACrms with compliance to latest safety standard IEC/EN/ES 60601-1 3rd edition for 2 x MOPP and they are approved for an operating altitude of up to 5000 m. The converters come along with the risk management file according ISO 14971.

With a high efficiency of up to 90% and highest grade components, the converters reliably operate in an ambient temperature range of –40°C up to 85°C while the design size is very small. A low leakage current of less than 2.5 µA qualifies them for BF (body floating) applications. The new models, in stock at Sager Electronics, have a wide 4:1 input voltage range and are available as single or dual output version. 

The new THM series medical DC/DC converters from TRACO Power are in stock at Sager Electronics. Click here to learn more.

About Sager Electronics
Sager Electronics, a wholly owned subsidiary of TTI Inc., a Berkshire Hathaway Inc. company, is a North American distributor of Interconnect, Power and Electromechanical components from leading manufacturers worldwide and a provider of value-add solutions. Grounded in over 130 years of innovation and service, Sager Electronics provides customers and suppliers a unique combination of operational excellence and innovative business solutions through its Distributing Confidence® business model. Headquartered in Middleborough, MA, Sager Electronics operates a national network of field sales representatives and power systems sales engineers, strategically located service centers across North America, and a value-add Power Solutions Center located in Carrollton, TX. To learn more about Sager, visit www.sager.com.

###

Links:
www.sager.com
www.power.sager.com
Sager Electronics on Facebook 
Sager Electronics on LinkedIn
Sager Electronics on YouTube 
Sager Electronics on Twitter
Sager Power Systems on Facebook
Sager Power Systems on Twitter

Contacts:
Maryellen Stack | Director of Marketing Communications  
19 Leona Drive, Middleborough, MA 02346 
tel 508-923-6678 | fax 508-923-6878
mstack@sager.com | www.sager.com

Jennifer O’Neil | Marketing Communications Specialist
19 Leona Drive, Middleborough, MA 02346 
tel 508-923-6762 | fax 508-923-6847
joneil@sager.com | www.sager.com

ECIAnow.org