TDK-Lambda DSP Series of AC-DC DIN Rail Power Supplies Now Shipping from Sager Electronics

NEW PRODUCT ANNOUNCEMENT

TDK-Lambda DSP series is now shipping from Sager ElectronicsMIDDLEBOROUGH, Mass. – October 1, 2018 – Sager Electronics, a leading North American distributor of Interconnect, Power and Electromechanical components and provider of value-add solutions, is now stocking TDK-Lambda’s DSP series of 7.5-100 Watt AC-DC, DIN Rail power supplies. 

The DSP series is a low profile AC-DC DIN Rail power supply designed for building and factory automation. It features operation from 90-264VAC with a Class II double insulated input (no ground connection required). The DSP series is UL508 listed and UL/EN60950-1 approved with certain models also approved to UL1310 Class 2. It has a wide operating temperature range with full load convection cooled operation up to 55°C. It is suitable for mounting on TS-35/7.5 and 15 DIN Rails as well as chassis mounting capability.

TDK-Lambda’s DSP series 7.5-100 Watt DIN Rail power supplies are in stock at Sager Electronics. To learn more, click here.

About Sager Electronics
Sager Electronics, a wholly owned subsidiary of TTI Inc., a Berkshire Hathaway Inc. company, is a North American distributor of Interconnect, Power and Electromechanical components from leading manufacturers worldwide and a provider of value-add solutions. Grounded in over 130 years of innovation and service, Sager Electronics provides customers and suppliers a unique combination of operational excellence and innovative business solutions through its Distributing Confidence® business model. Headquartered in Middleborough, MA, Sager Electronics operates a national network of field sales representatives and power systems sales engineers, strategically located service centers across North America, and a value-add Power Solutions Center located in Carrollton, TX. To learn more about Sager, visit www.sager.com.

###

Links:
www.sager.com
power.sager.com
Sager Electronics on Facebook 
Sager Electronics on LinkedIn
Sager Electronics on YouTube 
Sager Electronics on Twitter
Sager Power Systems on Facebook
Sager Power Systems on Twitter

Contacts:
Maryellen Stack | Director of Marketing Communications  
19 Leona Drive, Middleborough, MA 02346 
tel 508-923-6678 | fax 508-923-6878
mstack@sager.com | www.sager.com

Jennifer O’Neil | Marketing Communications Specialist
19 Leona Drive, Middleborough, MA 02346 
tel 508-923-6762 | fax 508-923-6847
joneil@sager.com | www.sager.com

Sager is a member of ECIA - ecianow.org