Sager Electronics Announces Immediate Availability of SDR Series AC-DC DIN Rail Power Supplies from MEAN WELL

NEW PRODUCT ANNOUNCEMENT

MEAN WELL's SDR Series is in stock at Sager ElectronicsMIDDLEBOROUGH, Mass. – October 8, 2018 – Sager Electronics, a leading North American distributor of Interconnect, Power and Electromechanical components and provider of value-add solutions, is now stocking MEAN WELL’s SDR Series 75-960 Watt AC-DC, DIN Rail power supplies. 

The SDR series is a slim size AC-DC DIN Rail power supply in a metal case that can be installed on a TS-35/7.5 or 15 mounting rail. It features operation from 90-264VAC (180-264VAC for SDR-960), with high efficiency up to 94% and low power dissipation. The design is UL508 (Industrial Control Equipment) and EN60950-1 approved while also meeting EN61000-6-2 (EN50082-2) industrial immunity levels. Most models have a built-in active PFC function as well as built-in DC OK relay contacts. 

The SDR series is an ideal power supply solution for industrial control systems, factory automation, and electro-mechanical applications.

MEAN WELL’s SDR series is in stock at Sager Electronics. Click here to learn more

About Sager Electronics
Sager Electronics, a wholly owned subsidiary of TTI Inc., a Berkshire Hathaway Inc. company, is a North American distributor of Interconnect, Power and Electromechanical components from leading manufacturers worldwide and a provider of value-add solutions. Grounded in over 130 years of innovation and service, Sager Electronics provides customers and suppliers a unique combination of operational excellence and innovative business solutions through its Distributing Confidence® business model. Headquartered in Middleborough, MA, Sager Electronics operates a national network of field sales representatives and power systems sales engineers, strategically located service centers across North America, and a value-add Power Solutions Center located in Carrollton, TX. To learn more about Sager, visit www.sager.com.

###

Links:
www.sager.com
power.sager.com
Sager Electronics on Facebook 
Sager Electronics on LinkedIn
Sager Electronics on YouTube 
Sager Electronics on Twitter
Sager Power Systems on Facebook
Sager Power Systems on Twitter

Contacts:
Maryellen Stack | Director of Marketing Communications  
19 Leona Drive, Middleborough, MA 02346 
tel 508-923-6678 | fax 508-923-6878
mstack@sager.com | www.sager.com

Jennifer O’Neil | Marketing Communications Specialist
19 Leona Drive, Middleborough, MA 02346 
tel 508-923-6762 | fax 508-923-6847
joneil@sager.com | www.sager.com

Sager is a member of ECIA - ecianow.org