Sager Electronics Announces Immediate Availability of LCM600 Series 600 Watt AC-DC Power Supplies from Artesyn

NEW PRODUCT ANNOUNCEMENT

Artesyn’s LCM600 Series 600 Watt front-end, AC-DC power suppliesMIDDLEBOROUGH, Mass. – November 19, 2018 – Sager Electronics, a leading North American distributor of Interconnect, Power and Electromechanical components and provider of value-add solutions, is now stocking Artesyn’s LCM600 Series 600 Watt front-end, AC-DC power supplies. 

The LCM600 series comprises five models, offering outputs of 12 V, 15 V, 24 V, 36 V or 48 V, together with an optional 5 V standby output. Each model accepts a universal input of 85–264 Vac and has a typical full load efficiency of 89%. 

Carrying industrial and medical safety approvals, the LCM600 series can deliver up to 600 watts and offer versatile bulk power for a wide variety of industrial, medical, military and process automation applications. They are especially suitable for systems that use a distributed power architecture (DPA) or point-of-load (POL) scheme. A built-in OR-ing FET allows up to 10 units to be connected in parallel for high current applications. 

Artesyn’s LCM600 series is in stock at Sager Electronics. Click here to learn more

About Sager Electronics
Sager Electronics, a wholly owned subsidiary of TTI Inc., a Berkshire Hathaway Inc. company, is a North American distributor of Interconnect, Power and Electromechanical components from leading manufacturers worldwide and a provider of value-add solutions. Grounded in over 130 years of innovation and service, Sager Electronics provides customers and suppliers a unique combination of operational excellence and innovative business solutions through its Distributing Confidence® business model. Headquartered in Middleborough, MA, Sager Electronics operates a national network of field sales representatives and power systems sales engineers, strategically located service centers across North America, and a value-add Power Solutions Center located in Carrollton, TX. To learn more about Sager, visit www.sager.com.

###

Links:
www.sager.com
power.sager.com
Sager Electronics on Facebook 
Sager Electronics on LinkedIn
Sager Electronics on YouTube 
Sager Electronics on Twitter
Sager Power Systems on Facebook
Sager Power Systems on Twitter

Contacts:
Maryellen Stack | Director of Marketing Communications  
19 Leona Drive, Middleborough, MA 02346 
tel 508-923-6678 | fax 508-923-6878
mstack@sager.com | www.sager.com

Jennifer O’Neil | Marketing Communications Specialist
19 Leona Drive, Middleborough, MA 02346 
tel 508-923-6762 | fax 508-923-6847
joneil@sager.com | www.sager.com

Sager is a member of ECIA - ecianow.org